EM 22.03.2.0 issue with Passwords for Email Accounts not being saved in Data Base.

Description 

On new installs of EM version 22.03.2.0 the passwords for emails settings to do not save to the DataBase.

Product 

EM 22.03.2.0

Steps to Reproduce 

  • Install exacqVision Enterprise Manager version 22.03.2.0
  • Set up Emails settings and apply password in EM settings.
  • Tested email with a IP camera disconnect.
  • Logs Seen in the WebServer EM logs:

Expected Results 

Once you enter the password and hit apply it should save the password.

Actual Results 

The Password is not saved to the database.

Solution

Roll back to version 22.03.1.0 or wait until the 22.06 release in June.

Ticket AESW-1150