Analytics not Shown as Alarm on Event Linking

Description 

If you are setting up an event linking using an Analytic Event Type this will not show as alarm in the status window.

Product 

  • exacqVision Client
  • exacqVision Server

Steps to Reproduce 

  • Select Event Linking.
  • Add a New Event and select Analytics.
  • Select your Event source, Action Type and Action Target.
  • Click Apply.

Expected Results 

The Status will change from Off to Alarm

Actual Results 

The Status always stays Off

Solution

This is as designed, many analytics triggers happen so fast that the Status on the Event Linking page never appears to change or it does so for only a split second.

Here is one way to verify it is working.

  • Change the Action Type to Log Event
  • Trigger the analytic
  • Search Events, there should be a red indicator in the timeline when the analytic triggered.