NIC Bonding with Windows Server 2016 is only available through Server Manager

Description

Servers with Windows 10 or Linux allow bonding to be configured via exacqVision Client.

However, servers with Windows Server 2016 currently do not. Instead, bonding must be configured via Windows Server Manager:

  • Start Server Manager.
  • Click “Local Server” in left pane of window.
  • Locate the “NIC Teaming” item in window, and click its “Disabled” link.
  • In the NIC Teaming window, you can add, remove, and edit bonds.

Product 

  • exacqVision Server
  • Windows Server 2016

Expected Results 

  • NIC Bonding options are available in the exacqVision Client

Actual Results 

  • NIC Bonding options are not available in the exacqVision Client on systems running Windows Server 2016.

Solution

  • Configure NIC bonding using the OS Server Manger

<br>