exacqVision 24.09 introduces the Remote Connections feature. This video for system administrators discusses the benefits of using Remote Connections as well as creating access codes for mobile users. This feature can be used with exacqVision Mobile 24.09 and above.<br><br>
Chapters:<br>
00:00 Intro<br>
00:33 Features of Remote Connections<br>
00:48 Network architecture<br>
01:54 Enable Remote Connectivity in the Client<br>
02:17 Mobile Optimized Streaming<br>
03:15 Creating access codes<br>
<br>