The ReadyRails that ship with exacqVision X-Series NVRs are designed to be toolless when used with server racks that have square or unthreaded round mounting holes on the rack uprights. The following guide describes how to adapt these rails, using tools, for use with rack uprights with threaded round screw holes.
- Examine the each end of the rail and take note of the pegs, as indicated in the illustration below.

- Insert a flathead screwdriver into the slot at the end of each peg and turn to remove the pegs. Repeat this on the opposite end of the rail.

- Remove the end plate. Repeat this at the opposite end of the rail.

- Fit the L-bracket on the end of the rail around the upright, facing outward. Use installer provided screws to secure the rail to the rack’s upright. Use the bottom of the bracket for front/rear alignment as the bracket holes are in different positions on the front and rear of the rail.

<br>