exacqVision Enterprise Manager (EM) provides a web-based dashboard to monitor system health, maximize surveillance uptime, manage large numbers of exacqVision system users, transfer camera licenses, and perform software updates across distributed exacqVision systems.
Some level of enterprise management may be performed via the exacqVision Client for Enterprise licensed NVRs. But Enterprise licensing allows you to use Enterprise Manager for no extra cost and take advantage of even more enterprise level features, such as:
- Automatic Failover, providing redundancy to NVRs
- Camera Inspection, a tool assisting with maintenance
- License Transfer, allowing the migration of camera licenses between NVRs, or allotted from a license pool
- Schedule singular or recurring configuration backups
Without Enterprise Manager
Without EM, a user with the exacqVision Client will connect to each exacqVision Server to manage system licenses, check cameras individually for issues, and update exacqVision software. Though it is possible to use the Enterprise page in the Client to manage users, configure notifications, and perform manual failovers. As the number of exacqVision Servers in your organization increases this can become much more time consuming and complex.

With Enterprise Manager
EM provides a singular web-based dashboard to instantly view the health status of hundreds of exacqVision Servers and camera connections across your entire organization. EM also provides the ability to configure spare systems providing automated Failover should a system encounter a power, storage, or maintenance issue. Transfer camera licenses between systems as needed or utilize a license pool to instantly add licenses to systems after hours.

Enterprise Manager also provides the ability to schedule tasks to take place in the future, or schedule recurring tasks, including configuration backups or software updates.

Enterprise Manager also allows administrators to logically group exacqVision Server instances to their choosing, such as by geographical area, building, or functional level. This provides better control of system and user management, as well as user access to system resources.
Each user’s exacqVision Desktop Client instance may also have their system lists automatically synchronized with EM permitting administrators to auto update the list of NVRs each user connects with.
Enterprise Manager communicates with each exacqVision Server using the same port the Desktop Client software uses, by default this is port 22609. Failover and Failback features utilize port 28744.
<br>