Guidance on Using USB Network Interface Adapters

On occasion, Exacq Support is asked about using a USB network interface (NIC) on their system. This is more frequently asked by those with smaller units which may have only one network interface and a user is attempting to add additional network interfaces to span networks or attempt to increase network throughput by bonding/teaming multiple NICs.

Regardless of the system model or size, Exacq does not support or test USB NICs.

Exacq Support will also not recommend any specific NICs for this usage. Even NICs connected externally using USB 3.0 or USB-C may encounter issues, therefore Exacq only supports internally connected network interface cards and does not troubleshoot issues with third-party devices added by users.

<br>