Remote Connections

exacqVision Server and Client versions 24.09 introduce our Remote Connections feature. This added feature currently only supports exacqVision Mobile. Connections for the Desktop Client, Exacq Mobile 3, or Web Client remain unchanged.

Products

  • exacqVision Server 24.09 and higher
  • exacqVision Client 24.09 and higher
  • exacqVision Mobile 24.09 and higher

What benefit does Remote Connections provide?

  • Ease of Setup – There is no need to configure routers to open ports and/or port forwarding, or configure additional software. This relay previously required configuration through the Web Service.
  • Authorization – Mobile users enter a single-use code provided by the exacqVision administrator to add a server connection.
  • Encryption – Enforces SSL/TLS connections.

Why don’t I have to configure port forwarding?

Traditionally, users outside of a LAN wishing to connect to services inside a LAN initiated the connection request. This can still be done if users choose this method.

However, when Remote Connectivity is enabled, the exacqVision software takes advantage of the fact that routers usually permit devices already inside the private network to initiate connections to outside services. This is what allows your web browser to load web pages without configuring port forwarding on your router. The exacqVision server establishes a secure connection to our Remote Connectivity agent. Users of the exacqVision Mobile app then connect to this Remote Connectivity agent. The Remote Connectivity agent handles the secure passing of data between the exacqVision Server and the user’s app.

What is this code users enter?

The Remote Connections feature provides another layer of security over just usernames and passwords. exacqVision administrators press a button within the exacqVision Client to create one or several single-use codes. A user wishing to add an exacqVision Server instance to their mobile app must enter the code provided by their system administrator before it expires (within 24hrs). The code is only needed for the initial connection to the server. Unless the user deletes the system from their mobile app, there is no need to enter a code the next time the app is used.

<br>

Related Articles

<br>