Lost or Forgotten Server Admin Password

Description

User passwords are stored in an encrypted form for your system security.

When non-administrative users lose/forget their credentials, a system administrator may login to reset these. However, if the credentials for the exacqVision Server administrator account have been lost/forgotten, these cannot be recovered.

Solution

In cases where administrative access to the system can longer be achieved, you must uninstall the exacqVision Server application and reinstall it.

  1. Begin the uninstallation process.<br><br>
  2. When prompted, opt to remove configuration files.<br><br>
  3. Reboot the machine to complete the full removal of all program files.<br><br>
  4. Log into the operating system with administrator privileges and re-install the exacqVision Server. This process will prompt you to create the credentials for the system administrator. <br><br>
  5. You will then need to add devices, add your system users, and configure the system.<br><br>
  6. When you have completed restoring the configuration, backup the system configuration using the Settings Export button on the Configure System > System tab.<br><br>