Description
exacqVision Edge is a complete video management system (VMS) software solution that runs directly on an IP camera and stores video to an microSD/SD card inserted in the camera.
Supported Devices
Use the filters on the exacqVision IP Camera Integration database to search for devices that support exacqVision Edge.
Installers
Download the appropriate installer for your device. Installers are listed by device model on the Software Downloads page.
Upload
Devices will vary by manufacturer and firmware version. The steps for Illustra IQ cameras are depicted below.
- Log into the device through the web browser interface. Out-of-box or factory defaulted devices will likely require steps to choose basic device settings and configure the administrator user account and credentials. Refer to the device’s documentation for details.<br><br>
- Locate the application management page within the device. Pictured below, Illustra IQ devices feature an Applications page from within the Applications menu.
<br><br>
- Select the installer file previously downloaded from Exacq.com to upload.
NOTE: Some cameras may not allow the application to upload until a microSD/SD card has been inserted, formated, and mounted.<br><br> - Uploaded applications typically begin running automatically after uploading. If the application does not appear to be running, use the device controls to start the application.
<br><br>
- The exacqVision Edge application is NOT licensed through the device itself. Disregard the License option within the camera’s web interface and proceed to the Licensing steps below.<br><br>
Licensing
- If you have not already done so, download and install the exacqVision Client software on a workstation you intend to you for viewing and management of the Edge device.<br><br>
- Within the exacqVision Client, use the cog wheel icon to access the Configuration screen.<br><br>
- Navigate to the Add Systems page and add the Edge VMS using the IP address of the camera you installed the Edge application on as the server Hostname/IP Address. Rather than entering the credentials to log into the camera, the system credentials will still be default. Enter the following for intial setup:
Username: admin
Password: admin256<br><br> - Upon initial connection with the default credentials the exacqVision software will prompt you to change the default credentials to those known only to you.<br><br>
- After changing the Edge Server credentials, you will see the exacqVision Server appear on your system tree to the left. Expand the server node and click to select the Configure System option.
<br><br>
- Select the System tab from the top of the Configure System page.<br><br>
- Within the License section of this page, either manually enter the license key or use the Import button options to upload the license key to authorize your Edge application.
<br><br>
- Navigate to the Add IP Cameras page and confirm the camera is now shown as connected in the IP Camera List. It is normal to see that the Address is 127.0.0.1 because the Edge application is running directly on the camera, thus it will display the local loopback address rather than the networked IP address of the camera.
<br><br>