Categories
exacqVision Integrations Other User Guides Knowledge Support Documentation Support Illustra Categories Products exacqVision Integrations

Illustra Body Worn Camera Indicators

The following is a reference for the meaning of several indicators that may appear on the Illustra Body Worn Camera screen during use.

  1. REC – indicates that the camera is recording to local storage<br><br>
  2. Information – pressing this icon on the camera’s touch screen displays the information panel with details about the camera<br><br>
  3. WiFi – when lit, this icon signifies that the camera is connected to a WiFi network<br><br>
  4. ONLINE – displayed when the device has a connection the Mobile Video Manager software and is ready for live streaming (live streaming requires a valid license)<br><br>
  5. Battery – indicates the current charge level<br><br>
  6. Alert – displayed when a configured action button has been pressed (See Integration Guide)<br><br>
  7. IR ENABLED – indicates the camera has enabled IR mode for poorly lit scenes<br><br>
  8. PRIVACY MODE ENABLED – camera wearer has enabled Privacy Mode, preventing Live streaming
    (Requires camera firmware 8.2.0.111 or higher)

<br>