Upgrading the Illustra Body Worn Camera Kiosk software versions 1.x to Kiosk versions 2.0 and above is NOT supported.
Kiosk 2.0 represents a completely re-written application which will not update previous 1.x installations.
Users who wish to upgrade to Kiosk 2.0 and above will need to remove the 1.x application and perform a fresh Kiosk install with 2.0 or higher.
See also: Illustra Body Worn Camera Kiosk 2.x Integration Guide
NOTE: A fresh installation of the Kiosk software will require rebuilding the Kiosk user accounts.
NOTE: When reconnecting to ExacqVision NVRs previously added users will no longer be associated with the previous user data as the underlying GUIDs will have changed.
<br>