Categories
Software Categories exacqVision Server Windows exacqVision Server Linux exacqVision Server Windows x64 exacqVision Server Linux x64 Knowledge Support Support exacqVision Server Categories Products

Operating System Release Notes

Systems built by Exacq utilize customized OS images for Windows and Ubuntu (Linux).

There may be instances where it is necessary to check the release version on an Exacq system. The release notes are contained within the operating system in a text file titled Release_Notes located on the root of the OS drive.

File path to OS release notes:

Windows – C:\Release_Notes.txt -or- C:\Release_Notes-Win10.txt
Ubuntu (Linux) – /Release_Notes.txt

<br>

NOTE: This file contains release notes for the operating system only. Refer to the Support Portal for ExacqVision software release notes.

<br>