Updating Camera Firmware When Using ExacqVision Edge

The ExacqVision Edge and Edge+ software runs a single-camera ExacqVision server instance directly on supported camera models.

To perform camera firmware updates, we recommend the following steps.

  1. Log into the camera’s web browser interface.<br><br>
  2. Stop the Edge server application.<br><br>
  3. Apply the firmware update following the firmware update instructions provided by the camera manufacturer.<br><br>
  4. Once the firmware update has completed, restart the Edge server application.<br><br>

<br>