Description
The following describes the currently available recording schedule types
Product
- C2C
- Cloudvue Gateway
Solution

Schedule Types
Motion
- Video recording is based on motion detection and is recorded both locally on the SD (C2C camera) or HDD (Gateway) and simultaneously in the cloud
Record
- Video recording is constant based on the schedule and is recorded both locally on the SD (C2C camera) or HDD (Gateway) and simultaneously in the cloud
Local Record, Cloud Motion
- Record all the time locally on SD (C2C camera) or HDD (Gateway), Motion detection is recorded on the cloud
Local Record, Cloud People Detection
- Record all the time locally on SD (C2C camera) or HDD (Gateway), People detection is recorded on the cloud
Local Record, Cloud Vehicle Detection
- Record all the time locally on SD (C2C camera) or HDD (Gateway), Vehicle detection is recorded on the cloud
NOTE: All cloud recording requires a subscription