ExacqVision Server

exacqVision Server is the core software application that implements the bulk of functionality offered by the exacqVision product line. The exacqVision Server connects to cameras, records video/audio/events data to the storage disks and makes it available for downstream consumption. This component does not have a user interface and requires a client software to be able to interact with it.

It can be installed on Windows or Ubuntu operating systems. It supports Exacq built hardware, third party hardware or VM environments.

By default, the server install comes with a free license for adding single camera. Please refer to this KB article on how to apply newly purchased licenses to exacqVision. Each license comes with software updates (“SSA”) support. The number of years of SSA support can be checked by following the instructions here.