Description: We have seen where ExacqVision is reporting a false alarm on the hardware page with systems that have the OS on RAID. The system drives show up RED in the GUI. This is a result from storcli reporting back “unkown” for the temperature.
Product: The option for OS on RAID is available for all Z-Series, S-Series and EM-Series. The A-Series it is only available in the 4U (R4A) and the Front accessible 2U (F2A).
Repro:
This was introduced in the last available retail key 22.12.1
Work Around:

Fix: Engineering is currently working on a fix