Cloudvue Analytics & Intelligence

Description

Cloudvue Intelligence provides access to whatever data analytics a particular camera may provide such as people and vehicle detection. Except for Motion, People and Vehicle Detection the camera must provide the desired analytic.

Products

  • Cloudvue Intelligence
  • C2C Cameras
  • C2G Cameras

Solution

Except for Motion, People Detection and Vehicle Detection, which are native to Cloudvue Intelligence, customers wanting to take advantage of  any of the other Intelligence features must ensure that the camera itself provides the desired analytic and the appropriate subscription has been applied.

NOTE:  The Cloudvue Intelligence feature is only available through the cloud interface.

Analytic Types and Descriptions

Cloudvue provides the following analytics natively but does require a “TCSVMSM – VMS Only” or greater subscription

Data TypeDescription
MotionDisplays a graph of detected motion for people or vehicles and can be set to daily or weekly.
People DetectionUsed to determine a human presence in the camera’s field of vision. This  feature must be enabled in the Settings before use
Vehicle DetectionUsed to determine a vehicle’s presence in the camera’s field of vision. This feature must be enabled in the Settings before use.

Cloudvue also supports the following analytics if provided by the camera and having a retention subscription

Data TypeDescription
People CountingDisplays a graph of the number of people entering, exiting, or both; and can be  set to daily, weekly, or monthly.
Heat MapsDisplays colored maps showing areas with frequent motion. The display can be set in intervals of 5 minutes to 24 hours.
Object Left BehindDisplays the number of events for an object left behind.
Object DetectionDisplays the number of events for detecting a known object.
LingerDisplays the number of events for linger. Linger is the duration of time a person stays within and around a defined area. It may also count a person walking around the area as lingering.
DwellDisplays the number of events for dwelling. Dwelling is the duration of time a person stays inside a defined area.
EnterDisplays the number of events for entering a defined area.
ExitDisplays the number of events for exiting a defined area.
CrowdDisplays the number of events for a crowd formation. Crowd formations specify the number of people necessary to constitute a crowd within a specific detection area.
QueueDisplays the number of events for queue formation. Queue formations specify the number of people necessary to form a line.
ThermalDisplays thermal imaging for infrared cameras for a given date and time

Additional Information

For a general explanation of Analytics and Intelligence see  Security Analytics & Intelligent Alerts Explained