DescriptionÂ
Definitions for exacqVision Server Recovery splash screens for systems using the refine boot loader.
Product
- exacqVision Server
Solution
Exacq systems have migrated to a new boot manager called refine. This new manager has a new look with the same and more functionality than the previous grub boot manager.
The new splash screen is icon driven and is displayed when UEFI booting from a deployment key or for 8 seconds. There are two versions of the screen with just slightly different functionality.
From a Deployment Key

- Deployment – This is the default action and will autorun if no other option is chosen.
- Wipe Machine – Will delete all RAID and all hard drive partition except the USB key.
- Clonezilla – Boots the system into a Clonezilla O.S. environment.
- Memory Test – Runs passmark memory test routine
From the O.S. – Linux 20.04, Windows LTSC , Windows Server 2018

- O.S – This is the default action and will boot the deployed O.S.
- Factory Restore – Will overwrite the current O.S. with the images that left the factory
- Clonezilla – Boots the system into a Clonezilla O.S. environment.
- Memory Test – Runs passmark memory test routine
<br>