Knowledge Base Article Template
Description
EM does not allow for the Root Group to select the option of Synchronization Conflict Resolution for Automatically Resolve Conflicts and remove Unauthorized Users as seen below.

Note: That even on a New Group- that the Group Name Needs to be provided and the Synchronization Conflict Resolution is able to be Applied.

Product
EM All Versions.
Solution
If this is seen on a Group with a Users in that Group of ROOT- then in order to select the Synchronization Conflict Resolution with Auto Resolve conflicts and remove unauthorized Users- you must create a New Group other than ROOT.