Cloudvue Custom View Users

Description 

A Cloudvue Custom View User is one which has not been assigned to any devices only to views. They are used to allow viewing rights such as live or view only to devices while not giving access to a device’s settings. If an existing Custom View User is removed from all views they will become orphaned and will appear to be hidden or missing.

Product 

  • Cloudvue
  • Cloudvue Mobile

Solution

Custom View Users Prerequisites

  • A view must exist to assign the Custom View User to see KB #13393 “Cloudvue Custom Views”
  • A Custom View User is not assigned to devices only to views
  • A Custom View User must be assigned to at least one view, or they will become orphaned
  • A Customer View User must be assigned a role, typically View Only or Live Only

Creating Custom View Users

  • Prerequisite:  A view must exist to assign the Custom View User
  • Login to Cloudvue as an Administrator
  • On the navigation tree select Settings
  • Select Users
  • Select Add User
  • Select Add New User
  • Fill out the “Add User” fields for the new user
  • Select the desired User Role (see below)
  • IMPORTANT:  By default an Assigned Device will be selected, uncheck ALL Assigned Devices
  • Assign one or more views
  • Select Save
  • A validation link will be sent to the new Custom View Users email address
  • They will need to follow the link in the email to complete the validation process before being able to login to Cloudvue

User Roles

  • View Only – User can view live and recorded video, Default Setting
  • Live Only – User can can view live video only
  • Enterprise –  User can view live and recorded video and change settings. They may also view but not change subscriptions
  • Billing Administrator – User Can view and edit subscriptions only

Orphaned Custom View Users

A Custom View User must be assigned to at least one view.  If removed from all views they will no longer display under Custom View Users nor appear as an assignable User when adding/editing Views

Recovering A Orphaned Custom View User

  • Login to Cloudvue as an Administrator
  • On the navigation tree select Settings
  • Select Add User
  • Select Add Existing User
  • Enter the existing Custom View Users email address
  • Assign them to one or more views and Save

Verify the Custom View User is no Longer Orphaned

  • On the Navigation Tree click on Account
  • The Custom View User should be listed under Custom View Users  NOTE: A page refresh may be necessary

Additional Information

Cloudvue Training Videos – Cloudvue Custom Views