*** INTERNAL USE ***
Description
exacqVision Server is not detecting motion from GSD cameras using the onvif plugin.
Product
- exacqVision Server 22.09
- Onvif Plugin (onvifnvcpi.json)
- GSD Cameras
- D2F28IP5MP-L
- D2FDA28IP5MP-L
Steps to Reproduce
- Add GSD camera to exacq server
- Configure motion on exacq and/or the camera
- Trigger motion
Expected Results
- Motion is detected in exacqVision
Actual Results
- Motion is not triggered in exacqVision
Solution
WARNING – This is temporary and will not survive an upgrade of exacqVision Server Software
Modify the “options” section for “manufacturer”: “GSD” in the onvifnvcpi.json


Note: See AES-69 for additional information