The processing loop performed *** passes and took ***ms to process the data.

The processing loop performed *** passes and took ***ms to process the data.

Description

A calculation is made by each camera plugin to determine if network operations ever took longer than 32ms. Once a minute, this data is logged. If it logs that it has “taken too long” this may indicate that the CPU is not able to keep up with the load.

Notes

Antivirus software may cause a delay in processing data.
The processing loop may take too long during heavy use, such as lots of reconnects to cameras, or many CGI commands (PTZ) and could be a sign that the system (CPU) is not powerful enough to process the current amount of camera data.