The processing loop has taken too long *** times. The longest time was ***ms for *** passes.

The processing loop has taken too long *** times. The longest time was ***ms for *** passes.

Description

A calculation is made by each camera plugin to determine if network operations ever took longer than 32ms. Once a minute, this data is logged. If it logs that it has “taken too long” this may indicate that the CPU is not able to keep up with the load.

Notes

A plugin that is not connected to any cameras will log this message once a minute and is not concerning.%BR%
Antivirus software may cause a delay in processing data.
The processing loop may take too long during heavy use, such as lots of reconnects to cameras, or many CGI commands (PTZ) and could be a sign that the system (CPU) is not powerful enough to process the current amount of camera data.