LDAP: Found keytab with SPN EDVR/%1 so no need to query server.

LDAP: Found keytab with SPN EDVR/%1 so no need to query server.

Description

%1 – This will likely be the Serial number or the MAC address of the Server.%BR%
Directory services found a keytab file containing an SPN so will not query AD for the SPN but use the SPN found in the keytab.

Notes

Linux only. %BR%
Can be problematic if the SPN in the keytab doesn’t exist. %BR%
This can happen when legacy setup used on the server with Centrify. Use ktutil interactive shell to list with “list” and remove with “delete_entry %slot%”