Failed to poll socket read/write status – WSAEFAULT. Failed to poll socket read/write status – WSAENOTSOCK

Failed to poll socket read/write status – WSAEFAULT. Failed to poll socket read/write status – WSAENOTSOCK

Description

In exacqVision Server 6.7.30, 6.7.31, and 6.8.1, the server will become unusable and the system might enter a reboot cycle if 63 or more clients are connected to the server at the same time. The server will log numerous instances this message.

Notes