camera detection is not available.

camera detection is not available.

Description

This could be caused by detection socket being used. Such as port 1900(UPnP) or 3702(ws-discovery) are being used by another application(use netstat) or mDNSResponder.exe is missing from the path.

Notes

If Onvif discovery failed in Windows environment, check to see if “Function Discovery Provider Host” and/or “Function Discovery Resource Publication” services are running. These two services also use port 3702 and will cause IPCamDetect to fail.