available system memory is low, throttling video

available system memory is low, throttling video

Description

In scenarios where the storage volume cannot keep up with the amount of data being recorded, video is buffered in memory in hopes that the storage volume can eventually catch up. This log indicates that 50% of the available RAM has been utilized. Once this log occurs, video is no longer being recorded.

Notes

If the system does catch back up and goes under 50% RAM usage, you’ll see ‘available system memory ok, not throttling video’.