How to Create a Video Wall in exacqVision Using VideoPush

Description 

The following instructions and resources can be used to configure a Video Wall using VideoPush in exacqVision.

Product 

  • exacqVision Client

Solution

Enable Video Push

Video Push must be enabled for each client which will be part of the Video Wall.

  1. Navigate to Config (Setup) page > Client > Video Push.
  2. Check the Enable Receiving Display.
  3. Give the instance a unique Display Name.

Layouts

If one of the provided templates does not reflect your video wall configuration, use Layouts to create a custom one.

  • Navigate to Config (Setup) page > Layouts.

Creating a Video Wall

  1. Navigate to Config (Setup) page > Video Walls.
  2. Select New.
  3. Enter a name for the video wall in the Name field.
  4. Select a layout option.
  5. Drag Available Applications i.e., the Video Push enabled client instances to the appropriate panel(s).
  6. Select Apply.

Send Video to The Video Wall Using VideoPush

  • Navigate to Live View.
  • Click the VideoPush icon in the toolbar.
  • Use the Mode, drop-down to select the Video Wall arrangement made in the previous steps.
  • Select Send.

<br>

Resources

Video Series Configuring a Video Wall https://www.youtube.com/watch?v=gHht8yKj5xE

Enabling Video Push exacqVision Client Users Manual https://docs.johnsoncontrols.com/exacq/r/Exacq/en-US/exacqVision-Client-User-Manual/22.06/Live-window/VideoPush-window

Layouts exacqVision Client Users Manual https://docs.johnsoncontrols.com/exacq/r/Exacq/en-US/exacqVision-Client-User-Manual/22.06/System-configuration/Layouts-window

Video Wall exacqVision Client Users Manualhttps://docs.johnsoncontrols.com/exacq/r/Exacq/en-US/exacqVision-Client-User-Manual/22.06/System-configuration/Video-Walls-window

Sending Video to the Video Wall exacqVision Client Users Manual https://docs.johnsoncontrols.com/exacq/r/Exacq/en-US/exacqVision-Client-User-Manual/22.06/Live-window/VideoPush-window/Sending-information-using-the-VideoPush-window