Exacq Unit Crashes When Backup is Imported

Description 

When importing a backup file to a NVR the system crashes the machine rendering it inaccessible. After a re-installation the import of the backup file once again crashes the system.
 

Product 

  • exacqVision Server

Steps to Reproduce 

  • Import backup file to the Exacq Server.

Expected Results 

  • Settings are imported and exacqVision Server continues normal operation 

Actual Results 

  • exacqVision Server service crashes and is not accessible

Solution

If the settings import correctly on a different system then check the disk(s) for corruption.

Linux #1702 – Manually Checking a Drive for Errors in Linux

Windows #10198 – Running Windows Chkdsk Command