Title
Resizing a Partition on Microsoft Windows
Description
If the capacity of a virtual drive has been increased; once the reconstruction has successfully completed, then it will be necessary to resize existing partitions before the operating system can utilize the additional space.
Product
- Microsoft Windows
- exacqVision Server
Overview
- Restart the NVR
- Stop exacqVision Server Service
- Launch Disk Management
- Resize the partition
- Start the exacqVision Server Service
- Check storage, previously recorded and new video
Restart the NVR
- Click the Windows Icon, the Power Icon, then choose Restart, the NVR will restart
Stop exacqVision Server Service
- Press Windows Key + R, the run box will open, type services.msc, click OK , the Services window will appear
- Locate and right-click on exacqVision Server, select Stop, a service control window will briefly appear then close once the service is stopped
- Leave the Services Window open
Disk Management
- Press Windows Key + R, the run box will open, type diskmgmt.msc, click OK, the Disk Management window will appear

- The Virtual Disk should show both the Primary Partition “Original Space” and Unallocated “New Space”
- Right-Click on the Virtual Disks Primary Partition, a context window will appear

- Select Extend Volume… , the Extend Volume Wizard will launch, click Next to continue


- Select the Disk to use space from and the amount of space in MB to extend, click Next
- Note: By default, the correct source and maximum available space should already be chosen.

- Review the proposed settings and click Back to modify, Finish to apply, or Cancel to abort, the wizard will close

- The Virtual Disk should now only have a single partition and show the new storage capacity
- Close Disk Management
Start exacqVision Server Service
- Open the Services window used previously
- Locate and right-click on exacqVision Server, select Start, a service control window will briefly appear then close once the service is started
- Close Services
exacqVision Client
- Open the exacqVision Client
- Navigate to the Drive Tab (Configuration > YOURSERVER > Storage)
- Verify the Capacity reported is correct and the status is Healthy
- Search for previously recorded video
- Verify current video is being recorded