Title
Deleting a MegaRAID Virtual Drive Using LSA (LSI Storage Authority)
Description
Instructions for deleting a MegaRAID virtual drive using LSA (LSI Storage Authority)
Product
- LSI Storage Authority
- MegaRAID
Prerequisite
Caution: The exacqVision Server service should be stopped before proceeding
Windows
- Press Windows Key+R, type services.msc in the run box then press enter
- Locate and Stop the exacqVision Server service
Linux
- Launch Terminal (Applications > Systems Tools > Terminal), execute the following command in the Terminal window
- sudo service edvrserver stop
Deleting a Virtual Drive
There can be several reason why you may wish to delete a virtual drive
- The virtual drive is failed and cannot be recovered
- Physical drive replacement to expand capacity
caution: All data on a virtual drive is lost when you delete it. Make sure to back up the data before you delete a virtual drive.
- Launch LSA from the desktop
- Enter the administrators username and password
- Use the drop down to Select Controller, the controller dashboard will appear
- From the Controller dashboard, select the Drive Groups Tab, click the + icon next to the drive group name (example DG_0). The Drive group will expand and the virtual and physical drives associated with the selected drive group appear.
- Select the virtual drive, a check will appear to the left of the drive group name and Element(s) Action will display available actions
- Select Element Action > Delete
- Select Confirm and click Yes, Delete, a message momentarily appears confirming that the virtual drive was deleted successfully, Drive Groups should show the following