Are DSCP/ToS set in exacqVision Server/Client Packet Headers

Title

Are DSCP/ToS set in exacqVision Server/Client Packet Headers

Description 

exacqVision Server/Client packets do not utilize DSCP/ToS (Differentiated Services Code Point (DSCP) Type of Service (Tos).

Product 

  • exacqVision Server
  • exacqVision Client

Description 

The ToS (type of service) or DiffServ (differentiated services) field in the IPv4 header, and the Traffic Class field in the IPv6 header are used to classify IP packets so that routers can make QoS (quality of service) decisions about what path packets should traverse across the network.