Illustra Camera Firmware Downgrades

Title

Illustra Camera Firmware Downgrades  

Description 

Once updated Illustra camera firmware cannot be downgraded.   

Product 

  • Illustra

Notice 

Previous versions of Illustra camera firmware are not available (nonnegotiable). Therefore, downgrading or rolling back to a previous firmware version should not be recommended or suggested as a troubleshooting step.

If there appears to be a compatibility issue and the following conditions are met, then the case should be escalated to L3 so they can work with engineering and product management towards resolution. 

  • Camera is on the most recent version of firmware 
  • exacqVision Server software is on the latest release