Description
Meanining of Cache Flush / Dirty Cache messages
Product
exacqVision Server
Information
This typically means that the RAID controller lost power/battery power during a write operation.
The RAID controller contains a small buffer for data being written to the hard drives. When the write has been confirmed, the cache is cleared.
Solution
If the machine lost power, this is a normal message, and is not of concern.
<br>