Description
When attempting to automatically import systems from a URL on startup the import fails.
Product
- exacqVision Server
Steps to Reproduce
- From the exacqVision Client navigate to the Add Systems page (Configuration > Add Systems)
- Select the Import/Export Tab Enable Automatic Import
- Select either URL on Startup or Synchronize with exacqVision Enterprise Manager
Expected Results
The system list is imported on startup
Actual Results
The list is not imported and an error similar to the following which includes “Reason: Could not open local temporary file” displays.

Solution
The currently logged in user does not have permissions to write to %userprofile%/AppData/Local/Temp. The system administrator will need to modify the users permissions to allow Read, Write and Delete privileges.