Title
Windows Remote Desktop Connection/RDP Not Working
Description
This has been observed after the Operating system has been updated to Windows 10 on exacqVision Servers using the Win10 upgrade kit.
Product
Windows 10 Remote Desktop Connection RDP
Solution
- Make sure you have run the Deploy clean-up script as per the exacqVision field recovery instructions.
- Check the desktop and if present double-click the Deployment Cleanup icon to launch the process.
- Once Cleanup has completed, the system will automatically reboot and take a factory image.
- When finished Remote Desktop Connection should work normally.
Note: This may also be applicable to systems which have had a full re-image performed.

Public Knowledge Base Article #