Description
A green icon indicates a secure (HTTPS) connection is being used for either or both the configuration connection to the device and/or the video stream.
Product
exacqVision Client
Solution
The green lock and gear icons are used as a visual indicators of the connection protocol being used by the camera. They can be found on the Cameras configuration page, the Add IP Cameras page and the Camera Recordings page.
- No Icon indicates standard connections are being used.
- Green gear indicates that the device is secure, but the video stream is standard.
- Green lock indicates that both the device and video stream are secure.