Title
Content Age
Description
The Content Age section is comprised of a Desired setting for setting an event trigger target and Oldest Content which shows storage information.
Product
exacqVision Client
Solution
Content Age

NOTE: This section is used to provide information and to set a target for triggering events. It does not restrict or remove stored data.
Desired: Select the target period of video that you would like to store data. If data is deleted before that target is reached, it creates an event that can trigger an action as configured on the Event Linking page.
Oldest Content: Indicates the age of the oldest video/data recorded on this system with the exception of any “At Least” storage rules or bookmarked video/data.