Adding Multi-Channel Encoders

Description

In order to accommodate more than 4 channels of video, many multi-channel encoders require the use of the “bank” IP plugin override. The cameras test records should indicate this in the Notes. 

Solution

  • 1st bank channels 1-4, no override required
  • 2nd bank channels 5-8, #bank=2
  • 3rd bank channels 9-12, #bank=3
  • 4th bank channels 13-16 #bank=4

For Example, assuming the cameras IP address is 192.168.1.1:

1st bank would be:192.168.1.1
2nd bank would be:192.168.1.1#bank=2
3rd bank would be:192.168.1.1#bank=3
4th bank would be:192.168.1.1#bank=4

<br>