Samsung Trigger Inputs Not working

Description

When the input is triggered on the camera, the input trigger in exacqVision client does not change state.  
Note: this effects Samsung SUNAPI2 cameras

Steps to Reproduce

  • Connect a switch to the cameras input trigger. 
  • In the camera
    • Configure Alarm output 1 (N.O.)/Pulse/5s
  • In the Client
    • add the camera using the Samsung plugin
    • Configure Trigger Input (Open)
    • Verify trigger status Normal and Connection Status Connected
  • Trigger the switch connected to the camera

Expected Result

  • Trigger Input 1’s trigger status changes to alarm in the client.

Actual Result

  • Status does not change in the client

Work Around

  • None at this time, but there will be a fix available in exacqVision Server 22.03.