Vulnerability Update for EM for Apache

IMPORTANT** Please look at the below notes before updating SOLR APACHE.

Starting with December 2021 (20.12 build) we have included an update for the Apache updates via a pop up during installation to update Apache to version 2.4.51.
IMPORTANT**
It is important to note that During the Apache upgrade it will backup the entire apache2 folder creating a folder apache2.old. The install does not modify any added files or folders as it will essentially unpack the new Apache upgrade zipped folder. This means during an Apache upgrade all configuration files will be unpacked and reconfigured according to a normal enterprise manager install. If there was custom modification done to any configuration files it will have to be manually migrated over to the new configuration files from the apache2.old directory.

The Dashboard will not update Existing Solr Apache so it is recommended that you update using the installers found on our site.
https://www.exacq.com/support/downloads.php


In addition 32 bit will no longer be supported for December release.

Ubuntu is not supported by the installer. A manual Upgrade is requires and will need to be performed.