exacqVision Enterprise Manager – Rules configured to send emails immediately are sending in batch instead

Issue:

Email rules configured to send email notifications immediately are being sent in batch instead.

This was introduced in exacqVision Enterprise Manager version 21.09.0 and will be fixed in the next release 21.12.x

see trac ticket #23249 for additional details.