Skip to content

Exacq

Support Portal CMS

USBDIO Modules connected to IP only NVRs will not have the PTZ use option

This is because that control should be provided by the encoder and the PTZ plugin is not installed.

<br>

Published November 1, 2021By Brian Lakin
Categorized as Knowledge Support, Support, exacqVision Server, Categories, exacqVision Hardware, Products Tagged Guest, PTZ, IP Server, Hybrid Systems, USBIO, 6492

Post navigation

Previous post

Exacq Mobile 3 App Crashing

Next post

Setting up Email Notifications to send a Start and a Stop email when the event starts and ends.

Recent Posts

  • Windows 7 Remote Connections
  • Associations Not Allowed to be saved as Momentary or Sustained Option
  • AVCostar (Arecont) AV20576RS camera model fails to decode H265 in ExacqVision
  • Illustra Edge Analytics
  • Hanwha Edge Analytics
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
  • Remote Connection