exacqVision Client direct access of Cloud-Drive storage does not list cameras by server configured camera names or display video time & date stamp.
Customers that attempt to review Cloud-Drive video from an off-site independent exacqVision Client pointed at the Cloud Drive URL https://exacq-gateway.cloudvue.com/v1/exacq with the proper credentials will be faced with the following limitations.
Limitations:
1. The exacqVision Client Search Cameras page shows a Cloud folder where the cameras are listed by a unique 6-digit name. The original server configured names are not associated in any way with the new camera names making it more difficult to locate a particular camera by the new name alone. This information is not stored in the cloud so the client has no way of accessing it.
- Cameras
- Cloud (Folder)
- 0123456789AB
- [ ] 361568
- [X] 361312
- [ ] 361569
- [ ] 361570
- [ ] 362080
- [ ] 361571
- 0123456789AB
- Cloud (Folder)
2. The exacqVision Client Search Cameras page has no On-Screen Display of the time & date stamp unlike when the Client connects through the server.

No Workaround:
- None available.
Unfortunately there is no immediate solution, neither of the two items are presently supported. The original camera names are not stored in the Cloud-Drive so the remote client has no way of accessing them. The video time & date stamp is not provided by the Cloud-Drive either. These items have been raised as feature enhancement requests to Cloud-Drive Product Line Management for future discussion and possible inclusion.