Audio Troubleshooting

Some cameras have audio inputs, which is not the same as having a built in microphone.

Sometimes you may also have to do a combination of tasks to get the audio to work correctly in Exacq.

External Microphones

  • Is audio scheduled to record
  • Is audio supported on the device?
  • Is audio enabled in the cameras Web GUI?
  • Are the Audio Inputs/Outputs enabled in the client?
  • Is the gain/sensitivity set either to high or low?
  • Is the stream profile setup correctly to allow Audio?
  • Is the recording format correct (JPEG, H.264, H.265)? *
  • Is the Codec supported (G.711, ACC)? *
  • Have you checked the exacqVision Server logs?
  • Has the cameras firmware version been tested? *
  • Do they need an Audio Bridge?
  • Is a powered microphone connected?
  • Is it connected to correct inputs?
  • Is the polarity correct?
  • Have you defaulted the device?

* Check the camera integration page