RtspServerPI may not be installed on Linux

Description

RTSP server is no longer seen in the tree under Add IP camera after upgrade to 20.12. If the server version is rolled back to 20.09 it can be seen again. This does not seem to affect windows installs​

Tested Version

20.12.x

Platform

Linux

Steps to reproduce

  • install/update server

Expected result

  • rtspserverpi is installed (in the plugins folder)

Actual result

  • rtspserverpi is not installed (is in plugin-store folder)
  • attempting to install through dpkg-reconfigure results in move error output

Work Around

  • manually install the plugin:
    sudo mv /usr/local/exacq/server/plugin-store/RtspServerPI.so /usr/local/exacq/server/plugins/rtspserverpi.so
  • restart the server