Temperature Scale:
Exacq defaults to Fahrenheit. Go into the Client Settings page and check the box for displaying the temps in Celsius

Client Temperature Display:
- Client / Server 21.06 or later is needed
- In live mode right-click on the thermal camera and select ‘View Analytics’
- The temperature will only be displayed when someone is above the high temperature threshold. It doesn’t work quite like the camera’s web GUI where it displays temps of everyone all the time. When a high temp is detected, the camera API then sends the face coordinates to Exacq allowing it to draw the bounding box, along with the temperature. It won’t display a “good” temp.
- Enhancement planned in future:
In the coming firmware update the API will add a low temp threshold for VMS to see, plus change some streaming temperatures so that the client should be able to display temps more closely to what’s seen in the camera web GUI.