Skip to content

Exacq

Support Portal CMS

Does Exacq use the Bosch BiPhase PTZ Protocol

No, Exacq uses the Bosch OSRD Protocol.  

To send BiPhase you will need a converter like the LTC8786, which connects to the DB9 RS232 port on the back of the unit.

Published May 7, 2021By Bhargav Atturu
Categorized as Knowledge Support, Support, Categories, Products, exacqVision Integrations Tagged Exacq Use of Bosch, BiPhase PTZ Protocol, Bosch Biphase, 5420, PTZ, Level2

Post navigation

Previous post

Identifying the Motherboard Installed in an exacqVision System

Next post

Verifying NTP on Linux system (8.04)

Recent Posts

  • Synchronize with Enterprise Manager authentication – Connectivity error:500
  • Exacq Mobile Application Views show Black Box
  • Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
  • FLIR Camera Motion Stops Recording Motion Events
  • exacqVision 25H1 Release Bulletin