Server crashes on start-up when audit directory cannot be created

Affected Versions

exacqVision Server 7.6 and earlier

<br>

Description

The server will crash on start-up if the audit directory does not exist and the server cannot create a valid audit directory. An example of this is when ‘audit’ is a symlink with an invalid target or a file exists with the same name as the directory, in this case ‘audit’

<br>

Workaround

Remove the file or symlink that is prohibiting the server from creating the directory.

<br>

Resolution

Update to exacqVision Server 7.8.0 or higher